Controller Properties
Use the
Controller Properties
dialog box to edit the properties of the controller. Studio 5000 Logix Designer
Firmware Supervisor
Firmware Supervisor status and error codes
Change the EtherNet IP Mode
Change the Lock state of a Safety application
Change the Safety Network Number (SNN)
Configure Internet Protocol settings
Configure the port settings
Additional Bus Capacitance out of range
Additional Fault Information
Additional Fault Information: 1756-HSC
Additional Fault Information: 1756-IF16, 1756-IF6I, 1756-IR6I, 1756-IT6I (Integer Mode)
Additional Fault Information: 1756-IF16, 1756-IF6I, 1756-IR6I, or 1756-IT6I (Floating Point Mode)
Additional Fault Information: 1756-OF6VI, 1756-OF6CI (Integer Mode)
Additional Fault Information: 1756-OF6VI, 1756-OF6CI (Floating Point Mode)
Additional Fault Information: 1756-PLS
Additional Fault Information: Discrete Input Modules
Additional Fault Information: Discrete Output Modules
Max size values must not exceed 15 for Non-EDT modules and 13 for EDT modules
Config assembly instance out of range
Config size is out of range
Cannot replace locked column
DANGER Changing Electronic Keying
DANGER Changing RPI
DANGER About to change RPI
DANGER Changing RPI and Electronic Keying
DANGER Configuration Changed
DANGER Redundancy with Unicast
DANGER Inhibiting Module Connection
DANGER Consumed tag configured for Unicast connections
DANGER Online Module Creation
DANGER Uninhibiting module
Disable keying
Electronic Key Passed Fault
Failed to create ControlNet file
Failed to create EtherNet/IP file
Failed to create the module
Failed to create the module
Failed to create the module
Failed to create the selected module
Failed to create module
Failed to inhibit the module connection
Failed to launch RSLogix Fieldbus Manager
Failed to launch RSNetWorx for ControlNet program file
Failed to launch RSNetWorx for EtherNet/IP program file
Failed to load the Configuration pages
Axes failed to access motion database
Failed to modify module properties
Failed to read the module status
Failed to read the required data
Failed to reconfigure the module
Failed name set - name is invalid
Failed name set - name is missing
Failed name set - name is too long
Host name or IP address conflict
If controllers are sharing module
Input assembly instance out of range
Input size is out of range
Input status size is out of range
Invalid IP address
Invalid operation
Major Fault State
Major fault types and codes
Minor fault types and codes
Module deleted by another session
Module Fault Icon
Module Faults
Module Faults: 16#0000 - 16#00ff
Module Faults: 16#0100 - 16#01ff
Module Faults: 16#0200 - 16#02ff
Module Faults: 16#0300 - 16#03ff
Module Faults: 16#0800 - 16#08ff
Module Faults: 16#fd00 - 16#fdff
Module Faults: 16#fe00 - 16#feff
Module Faults: 16#ff00 - 16#ffff
Motor catalog number error
Online command failed
Output assembly out of range
Output size is out of range
Status input assembly out of range
Status output assembly out of range
SynchLink Transmit Axis tags deleted
SynchLink tags deleted
Low Application Memory
Low graphic resources
Clear faults
Estimate memory requirements offline for controllers with divided memory
Perform Nonvolatile Memory Operations
Potential loss of project documentation, extended properties, and custom properties
View the maximum and used Ethernet nodes for a controller
View runtime memory usage for controllers with divided memory
View Safety Status and Signature
Logix Designer Application Capabilities and Redundancy State
Editing Controller Properties
CIP Sync
About IEEE 1588 PTP (Precision Time Protocol)
Runtime Controller Configuration and Status
Logix Designer running low on graphics resources
Adjust security settings to allow launch of Logix Designer application from a remote computer
Configure Changes to Detect dialog box
Advanced Redundancy Configuration dialog box
Cannot disable more than one port on the controller
Ratio between Continuous Task and Service Communication
Can't modify controller properties
Can't update the CST master setting
Clear the Alarm Log
Configure the System Overhead Time Slice
Configure a Controller Fault Handler program
Configure a Power-Up Handler program
Configure Advanced Redundancy Configuration options
Configure Redundancy
Enable front-port crossload in a redundant project
Configure Sequential Function Chart routine execution
Configuring the Expansion I/O in the Controller Properties dialog
Confirm change to controller type
Controller Date and Time dialog box
Failed to modify the controller properties
Coordinated System Time Master (CST) converted to Enable Time Synchronization
Could not clear the minor fault log. No message available for error
Could not set/clear the minor fault bit. No message available for error.
Could not store to nonvolatile memory
DANGER. Disabling Automatic Output Processing prevents outputs from being sent automatically to the I/O module
DANGER. Disabling Supervisor Mode may disrupt online communications
Date out of range
Day out of range
Differences between RSSecurity Server and FactoryTalk Security
Error could not load from nonvolatile memory
Failed to change the controller configuration
Failed to clear the project controller path. Access is denied.
Failed to modify communications configuration
Failed to modify priority level. Index out of range.
Failed to modify the ASCII Protocol configuration
Failed to modify the DH485 Protocol configuration
Failed to modify download project documentation configuration
Failed to modify the Internet Protocol configuration
Failed to modify the passthrough configuration
Failed to modify the System Protocol properties
Failed to modify the controller properties
Failed to set the CV High Limit and the CV Low Limit percent values. The CV Low Limit is greater than the CV High Limit.
Handle fault conditions
Hour out of range
How do I open the Controller Properties dialog box
Minute out of range
Online command failed
Partner
Partner Connection Not Established
Port Diagnostics dialog box parameters
Primary Control Chassis
Private users
Redundancy System Update
Reset the port diagnostic counters
Running low on graphics resources
Running low on memory
Second out of range
Secondary Control Chassis
Select Recent Communications Path Dialog Overview
Select clock priorities
Changing EtherNet/IP Mode dialog box
Failed to change the EtherNet/IP Mode
Failed to change the online EtherNet/IP Mode
Standby Secondary
Synchronized Primary
Synchronized Secondary
No support of embedded Ethernet port with redundancy
No support of Ethernet port configured modules with redundancy
Port Diagnostics dialog box
Unable to open properties
When redundancy is enabled, Event tasks must be deleted from the project and no tasks can be inhibited
Apply the Protect Signature in Run Mode change?
Find in Logical Organizer command
Provide Feedback