Confirm change to controller type

After selecting
Change Type
in the
Change Controller
dialog box, confirm to change the controller type.
For ControlLogix 5590 controllers, after changing the
Safety Enabled
checkbox setting on the Controller Properties > Safety tab dialog box, confirm to enable or disable safety for the controller.
Carefully read the consequences of the change that are listed on this screen. Then select
Yes
to continue with the change or
No
to keep using the existing controller.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal