Failed to set the CV High Limit and the CV Low Limit percent values. The CV Low Limit is greater than the CV High Limit.

You pressed the OK or Apply button on the Configuration dialog box and the CV Min and CV Max values are invalid. Enter a CV Low Limit that is less than the CV High Limit.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal