Failed to create module
A problem occurred when you installed the module. The error message you receive indicates one of these conditions:
Libraries not registered.
The libraries are not registered. Please contact Technical Support.
A Redundancy system.
Redundant systems have a limited set of supported local and remote devices. Some devices are restricted based on their major revision. Remove unsupported devices or select a major revision which is supported, or disable redundancy. For more details, see the
ControlLogix Redundancy User Manual
, publication no. 1756-UM535
.Provide Feedback