Failed name set - name is missing
There was a problem setting the name of the module. No name was supplied.
This module requires a name. Enter a name using the format defined by the IEC-61131 Name standard.
Provide Feedback