Electronic Key Passed Fault
Despite passing the electronic keying test, the module being connected to does not have the same features or settings as the module specified in the I/O configuration tree and does not support the connection or service being attempted.
Check the module in use and verify that it exactly matches the module specified in the I/O
configuration tree of the Logix Designer application.
Provide Feedback