DANGER Changing RPI and Electronic Keying
Changing the RPI and Electronic Keying selections interrupts the connection to the device. If an I/O connection to a device is interrupted, the result can be a loss of data.
For more information on Electronic Keying, see Electronic Keying in Logix 5000 Control Systems Application Technique, publication LOGIX-AT001.
Click
OK
to perform the operation or Cancel
to cancel the operation.Provide Feedback