Cannot replace locked column

In the Tag Editor, the Tag Name and Produce column positions are locked; in the Data Monitor, the Tag Name column position is locked. Because these columns are locked, replacing the position of a locked column is not permitted.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal