Configure Internet Explorer for FactoryTalk Historian ME

In this section, you will learn how to configure Internet Explorer to work with FactoryTalk Historian ME websites.
TIP:
Support for Internet Explorer may be removed in a future release. Please update Series B to FRN 5.203 in order for the module to support more modern web browsers like Chrome and Edge.
The following browsers are supported:
  • Microsoft®
    Internet Explorer®
    11
The following operating systems are supported:
  • Windows®
    10
  • Windows Server®
    2019
  • Windows Server
    2016
  • Windows Server
    2012
    TIP:
    This section has been prepared assuming that you access the module by typing its IP address in the browser. If you access the module by typing the Fully Qualified Domain Name (FQDN) of the module in the browser, follow the instructions, and type the FQDN instead of the IP address.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal