Add the module site to Local intranet or Trusted sites
By default, if you visit a website by entering an IP address in the browser, it is identified as a website in the
Internet
security zone. Thus, if you open the FactoryTalk Historian ME client website using the IP address of the module, the website will be added to the Internet
security zone. However, to work with the FactoryTalk Historian ME client website, you have to change the security zone and add the module website to:By default, the
Local intranet
security level is medium-low. The Trusted sites
security level is medium.The medium-low security level is the same as the medium level but without prompts. Use the
Local intranet
zone if you do not want to be prompted when the content of the page is run.
TIP:
Internet security is subject to the security policy and it may be changed by the system administrators. The zone that you choose depends on the corporate Internet security policy.
Provide Feedback