Add the module website to the Trusted sites security zone
To add the module website to the Trusted sites zone
- Open the FactoryTalk Historian ME website using the IP address of the module.
- On theToolsmenu, clickInternet Options.TheInternet Optionsdialog box appears.TIP:If the top menu is not visible, press the left Alt key on your keyboard to bring up the top menu.
- Click theSecuritytab, and then selectTrusted sites.
- ClickSites.TheTrusted sitesdialog box appears.
- Verify that in theAdd this website to the zonetext box there is a URL of your module site, and then clickAdd.The URL of the module website appears in theWebsiteslist. Depending on the security protocol used to communicate with the module, the website URL will be prepended by thehttpsprefix. You need to add the URL, starting with thehttpsprefix, to theWebsiteslist.
- In theAdd this website to the zonetext box, type the IP address of the module with the prefix other than the one of the URLs already added to theWebsiteslist, and then clickAdd.Both URLs for the module website appear in theWebsiteslist.
- ClickClose, and then clickOK.
Provide Feedback