Internet Explorer configuration checklist
To configure Internet Explorer to work with FactoryTalk Historian ME websites, you need to perform the following actions:
- Enable the Initialize and script ActiveX controls not marked as safe for scripting option for the particular security zone.
- If you are using Internet Explorer 10, perform the following in the F12 developer tools:
- Select theScript,Pop-Up Blocker, orCSSoption on theDisablemenu.
- Clear theDisable imagesoption on theImagesmenu.
- Clear theDisable cookiesoption on theCachemenu.
Provide Feedback