Add a registry entry for exporting files to Excel

In some versions of Internet Explorer, there is an issue when you try to export a file to Excel on the
System Log
page of the FactoryTalk Historian ME client website, and the
Save As
dialog box does not appear.
To fix this issue, you must add the
[HKEY_CLASSES_ROOT\.csv] "PerceivedType"="document"
registry value for the .csv document type.
For more information about editing registry entries, refer to the Microsoft documentation.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal