Install the module certificate in Internet Explorer
If you are using a secure communication protocol (HTTPS) to communicate with the
FactoryTalk Historian ME websites, you need to install a security certificate in the
browser. For more information on the security settings available for FactoryTalk Historian
ME, see Manage security.
To install the module certificate in Internet Explorer
- Open the FactoryTalk Historian ME website using the HTTPS protocol and the IP address of the module (for example,https://10.76.38.162). You should see a screen like the one below because your self-signed certificate is not trusted.
- ClickContinue to this website (not recommended).The website is loaded and the address bar is shown in red with a "Certificate error" message in the security status bar next to it.
- ClickCertificate error.TheCertificate Invalidmessage appears.
- ClickView certificates.TheCertificatedialog box appears with information that the website's certificate is not trusted.
- Verify the certificate:
- Verify the value in theIssued tofield corresponds to your module IP or hostname.
- Verify the value in theValid to...field. Check if the certificate has not expired.
- If the certificate has not expired, clickInstall Certificate, and follow the steps in theCertificate Import Wizardto complete the process.For details, see Install the certificate using the Certificate Import Wizard.If you do not see theInstall Certificatebutton:
- Close Internet Explorer.
- Right-click the Internet Explorer icon, and clickRun as administrator.
- Open the FactoryTalk Historian ME website again, and repeat steps 1-6.
Provide Feedback