Verify the browser configuration using the F12 developer tools
The F12 developer tools allow you to toggle certain browser features on and off. These features allow you to properly display the content of the FactoryTalk Historian ME websites. Verifying the browser configuration using the developer tools is especially recommended:
- If you are using Internet Explorer 10 or earlier.
- If you are using Windows Server (for more information, see Configure Internet Explorer on Windows Server).
To verify the browser configuration using the developer tools
- Go to the FactoryTalk Historian ME website, and then press F12.
- On theDisablemenu, make sure that theScript,Pop-Up Blocker, andCSSoptions are cleared.
- On theImagesmenu, make sure that theDisable imagesoption is cleared.
- On theCachemenu, make sure that theDisable cookiesoption is cleared.
Provide Feedback