Enable Active X controls

When you are interacting with the FactoryTalk Historian ME websites, scripts are run on the page to complete various actions (for example, uploading a file on the
Upload Management
page). For this reason, FactoryTalk Historian ME requires that you customize the security level and enable the
Initialize and script ActiveX controls not marked as safe for scripting
option.
To enable Active X controls
  1. In the
    Internet Options
    dialog box, click the
    Security
    tab, and then click
    Custom level
    .
    The
    Security Settings
    dialog box appears.
  2. Under
    Settings
    , browse to the
    ActiveX controls and plug-ins
    node.
  3. Under
    Initialize and script ActiveX controls not marked as safe for scripting
    , click
    Enable
    , and then click
    OK
    .
    TIP:
    See Internet Explorer security zone settings for a list of all security zone settings configured for FactoryTalk Historian ME websites.
  4. Click
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal