Enable the XML DOM Document add-on
The FactoryTalk Historian ME website requires the Microsoft XML DOM Document add-on to communicate with the module and send data. Make sure that the add-on is installed and enabled.
To enable the XML DOM Document add-on
- On theToolsmenu, clickManage add-ons.TheManage Add-onsdialog box appears.TIP:If the top menu is not visible, press the left Alt key on your keyboard to bring up the top menu.
- UnderMicrosoft Corporation, verify that all XML DOM Document add-ons are enabled.
- If the add-ons are disabled, underShow, selectAll add-ons.
- UnderMicrosoft Corporation, click each XML DOM Document add-on, and then clickEnable.
- ClickClose.
Provide Feedback