Points view

Use the
Points
view to:
  • Specify the behavior of each output when the controller transitions to Program mode.
  • Specify the behavior of each output when a communication fault occurs and the device enters Communications Fault mode.
  • If supported, verify the state of an output.
  • If supported, enable the detection of the absence of field wiring or a missing load.
  • If supported, enable the detection of the loss of field power to the device.
  • If supported, enable diagnostic latching.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal