Enable diagnostic latching
Configure each point on the device to latch diagnostic members so that they remain set after they are triggered.
Prerequisites
- Make sure that the connection is configured for Data.
To enable diagnostic latching
- On the tab for the device, selectPoints.
- In thePointsview, in theEnable Diagnostics Latchingcolumn, enable diagnostic latching by selecting the checkbox of each point.TIP: Select or clear all checkboxes in a column at once by selecting or clearing the checkbox in the header of each column.
- SelectOKto save the changes.
Provide Feedback