Points view parameters
The
Points
view includes these parameters:
TIP:
If the connection is configured for Rack, the diagnostic configuration and I/O data are not supported. If the connection is configured for Data, the diagnostic configuration and I/O data are supported. The supported diagnostics are determined by the catalog number.
Parameter | Description |
|---|---|
Output State During Program Mode | Specifies the behavior of each output when the controller transitions to Program mode.
|
Output State During Fault Mode | Specifies the behavior of the output of each point after a communication fault occurs and the device enters Communications Fault mode.
|
Enable Diagnostics for Output Verify | Verifies that the actual state of an output is the same as the commanded state, when the commanded state was ON. A fault is detected when the output point is erroneously off after is was commanded to be ON. This diagnostic is available only when an output point is commanded to be ON. |
Enable Diagnostics for No Load | Enables the detection of the absence of field wiring or a missing load. This diagnostic is enabled only when an output point is commanded to be OFF. |
Enable Diagnostics for Field Power Loss | Enables the detection of the loss of field power to the digital output device. This diagnostic is available only for 1756 Digital AC diagnostic output devices. |
Enable Diagnostics Latching | Configures each point on the device to latch diagnostic members so that they remain set after they are triggered. |
Pulse Test | Verifies output circuit functionality without changing the state of the output load device. The pulse test turns on the output and ensures that it comes on when the command is issued. The device detects the change in the output before the output load device has enough time to change its state. |
When Communication Fails in Program Mode | Specifies the behavior of the outputs if communications fail in Program mode:
|
Provide Feedback