Specify the output state if communication fails in Program mode

Specify the state of each output point when a communication failure occurs while the controller is in Program mode.
To specify the output state if communication fails in Program mode
  1. On the tab for the device, select
    Points
    .
  2. In the
    Points
    view, in the
    When Communication Fails in Program Mode
    section, select one of these options:
    • Leave outputs in Program Mode state
    • Change outputs to Fault Mode state
  3. Select
    OK
    to save the changes.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal