Specify the output state when the controller is in Program mode

Specify the behavior of each output point when the controller transitions to Program mode. While in Program mode, outputs from the controller are ignored, and the output behaves according to the behavior selected.
To specify the output state when the controller is in Program mode
  1. On the tab for the device, select
    Points
    .
  2. In the
    Points
    view, in the
    Output State During > Program Mode
    column, for each output point, select one of these options:
    • Off.
      Output becomes 0 or OFF in Program mode.
    • On.
      Output becomes 1 or ON in Program mode.
    • Hold.
      Output maintains last state in Program mode.
  3. Select
    OK
    to save the changes.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal