Specify the output state when the device is in Fault mode

Specify the behavior of each output point when a communication fault occurs and the device enters Communications Fault mode.
To specify the output state when the device is in Fault mode
  1. On the tab for the device, select
    Points
    .
  2. In the
    Points
    view, in the
    Output State During > Fault Mode
    column, for each output point, select one of these options:
    • Off.
      Output becomes 0 or OFF in Communications Fault mode.
    • On.
      Output becomes 1 or ON in Communications Fault mode.
    • Hold.
      Output maintains current level in Communications Fault mode.
  3. Select
    OK
    to save the changes.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal