Verify output state
Verify that the actual state of an output is the same as the commanded state, when the commanded state was ON. A fault is detected when the output point is erroneously OFF after it has been commanded to be ON. This diagnostic is available only when an output point is commanded to be ON.
Prerequisites
- Make sure that the connection is configured for Data.
To verify output state
- On the tab for the device, selectPoints.
- In thePointsview, in theEnable Diagnostics for Output Verifycolumn, select the checkbox for each point to verify.
- SelectOKto save the changes.
Provide Feedback