Detect the absence of field wiring or load

Enable detection of the absence of field wiring or a missing load. This diagnostic is enabled only when an output point is commanded to be OFF.
Prerequisites
  • Make sure that the connection is configured for Data.
To detect the absence of field wiring or load
  1. On the tab for the device, select
    Points
    .
  2. In the
    Points
    view, in the
    Enable Diagnostics for No Load
    column, select the checkbox for each output point to enable No Load detection.
  3. Select
    OK
    to save the changes.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal