Migrate RSSecurity to FactoryTalk Security

Migrate from RSSecurity to
FactoryTalk® Security
to centralize users, groups, permissions, policies, and actions in a
FactoryTalk Security
Directory.
Prerequisites
  1. Back up the existing RSSecurity database.
  2. Run
    FactoryTalk® Administration Console
    and back up your existing
    FactoryTalk® Directory
    and System folder.
To migrate RSSecurity to
FactoryTalk Security
  1. (optional) If the current system uses
    FactoryTalk® Automation Platform
    2.00, update the
    FactoryTalk Directory
    with a new set of actions for
    Logix Designer
    application
    .
    FactoryTalk® Services Platform
    2.10 (CPR 9) or later automatically contains these new actions.
  2. Use
    FactoryTalk Security
    Import
    to import an RSSecurity database into the
    FactoryTalk Directory
    .
    If all of the computers on your network have been upgraded to
    FactoryTalk Services Platform
    2.10 (CPR 9) or later, the import retains the original action groups and specifies resource grouping during migration.
  3. (optional) Install the
    RSSecurity Emulator
    to allow
    FactoryTalk Directory
    to emulate an RSSecurity Server. This allows existing RSSecurity clients, for example, the
    RSLogix
    family of software to connect to
    FactoryTalk Directory
    .
  4. Use either
    FactoryTalk® Administration Console
    or
    FactoryTalk View Studio
    to view and edit resources.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal