FactoryTalk Security Resource Group Import
How do I open
FactoryTalk Security
Resource Group Import?
To open
FactoryTalk Security
Resource Group Import:- SelectStart > All Programs > Rockwell Software > FactoryTalk Tools > Import RSSecurity Configuration.
- Complete theImport an RSSecurity databasedialog box.
- Complete theRSSecurity Migration Utilitydialog box, and then clickNext.
Use to import a resource group into a
FactoryTalk Security
Resource Group ImportFactoryTalk Directory
as either individual resources or grouped under either an application or area.To associate a group of resources with an application or area
- Right-click the resource group name, selectAdd Group to Area, and then navigate to the application or area. You cannot select the Network or Local directory object -- the highest object in the tree.
To import resources as individual items
- Leave theApplicationorAreacolumn blank, and then selectOK. Imported resources appear in theNetworks and Devicesfolder of theFactoryTalk Directory.
To remove a set of resources from a particular area of the FactoryTalk Directory
- Right-click the resource group name and then selectRemove group from area.TIP:Importing newLogix Designerapplication resources into aFactoryTalk Directoryadds a set of securable actions to the Networks and Devices folder. The security settings associated with these actions affect the default security settings applied to any newRSLogix 5000device added to theFactoryTalksystem. Verify the security settings of any newRSLogix 5000device before deploying it in a production system.
Provide Feedback