Import an RSSecurity database
Both RSSecurity Network and Local Edition databases can be imported into either a
FactoryTalk
Network Directory or a FactoryTalk
Local Directory. Use the FactoryTalk® Security
Import tool to import an RSSecurity Server database into a FactoryTalk Directory
. Import the RSSecurity Server database into either a FactoryTalk
Local Directory or a Network Directory or allow the FactoryTalk Security
Import tool to determine which directory to import into automatically. FactoryTalk
Network Directory and Local Directory are completely separate, even when configured on the same computer. If you are using both directories, set up security in each directory separately. Project information and security settings remain cannot be shared between directories.Imported users, actions and resources can be edited in
FactoryTalk Administration Console
or FactoryTalk View Studio
.Prerequisites
- Back up your existing RSSecurity database.
- RunFactoryTalk® Administration Consoleand back up your existingFactoryTalk Directoryand System folder.
To import an RSSecurity Server database
- On a computer where theFactoryTalkplatform is installed, go toRockwell Software > FactoryTalk Toolsand runImport RSSecurity Configuration.
- In, selectFactoryTalk SecurityImportBrowse, choose a backup database to import, and then selectOpen.
- In, select import options, and then selectFactoryTalk SecurityImportOK.
- Confirm theFactoryTalk Directoryhas been backed up:
- If theFactoryTalk Directoryis backed up, selectYes.
- If theFactoryTalk Directoryis not backed up, selectNo, and then selectCancel. Back up the directory, and then begin the import process again.
- When prompted, log on toFactoryTalkusing the account user name and password for a member of thegroup.FactoryTalk SecurityAdministrators
- If the computer:
- hasinstalled, RSSecurity actions and resources are imported automatically as individual items, and not as part of any group. Action group and resource grouping features are not supported inFactoryTalk Automation Platform2.00 (CPR 7)FactoryTalk Automation Platform2.00.
- hasinstalled,FactoryTalk Services Platform2.10 (CPR 9) or laterRSSecurity Migration Utilityappears. Choose an action and resource group option, then selectOK.
- Import RSSecurity action groups and resource groups asSelect if all of the computers in theFactoryTalkaction groups and resource groups:FactoryTalksystem are runningFactoryTalk Services Platform2.10 or later.
- Import RSSecurity action groups or resource groups as individual actions or resources:Select if computers in yourFactoryTalksystem are runningFactoryTalk Automation Platform2.00 or earlier.
- (optional) IfImport Issue Resolutionappears, resolve the conflicts, and then selectContinue.
- (optional) Ifappears, choose to import a resource group into aFactoryTalk SecurityResource Group ImportFactoryTalk Directoryas either individual resources or grouped within a specific application or area.
Provide Feedback