Back up a FactoryTalk Directory
Back up a
FactoryTalk Directory
to move a development FactoryTalk
system to a run-time FactoryTalk
system, or to create a backup for disaster
recovery purposes.When you back up an entire
FactoryTalk Directory
, the archive file includes: - All objects, references to objects held within theFactoryTalk Directory, and the security authority identifier. The archive file does not contain project files that are specific to individual products.IMPORTANT: The archive file does not contain project files that are specific to individual products.
- All applications associated with that directory. Typically an application contains areas (in a network directory), resource grouping information, and references to data servers, device servers, alarm servers, and HMI servers.
- The System folder, which includes a list of user, computer, and group accounts, passwords, system policy settings, product policy settings, system security settings, action groups, and alarm and event database definitions.TIP:To back up aFactoryTalk Directorywithout its security authority identifier, or to back up only the security authority identifier, selectTools > Security Authority Identifier. InModify Security Authority Identifier, selectBackupand follow the on-screen instructions.
Prerequisites
- Obtain the security permissions needed to perform backup and restore operations. OpenSystem>Policies>System Policies, and openUser Rights Assignment. UnderBackup and Restore > Backup and restore directory contentsselectConfigure Securityand verify access permissions have been granted.
To back up a
FactoryTalk Directory
- InFactoryTalk Administration ConsoleExplorer, right-click theNetworkorLocalDirectoryicon, then selectBackup.
- InSpecify archive name, use the default name or type another name for the backup file.TIP:It is recommended to not change the default archive name. The default name contains the leading digits of the security authority identifier which allows you to easily identify the archive file associated with a specific directory.
- InSpecify archive location, use the default archive location or useBrowseto open theBrowse for Folderwindow and specify another location.
- InBackup Contents:
- Selectto back up the entireFactoryTalk DirectoryconfigurationFactoryTalk Directory.
- (optional) Selectto back up shortcut and driver configurations.FactoryTalk Linxconfiguration
- (optional) Selectto back up server configuration, UA Server Endpoint settings, Advanced Settings, and UA Tag List configuration inFactoryTalk Linx GatewayconfigurationFactoryTalk Linx Gateway.
- To encrypt your archive file, select theEncrypt file contentscheckbox, and then enter the same passphrase in thePassphraseandConfirm passphrasefields. If you clear this checkbox, your backup archive file will not be encrypted or protected.Encrypt file contentsis not available if your operating system does not support the proper level of encryption.IMPORTANT:Remember the passphrase when choosing to encrypt the file contents. The archive file cannot be restored without the correct passphrase.
- SelectOK.Unless a different file name was specified,FactoryTalk Administration Consolecreates a directory backup file with its current security authority identifier in the default location or in the location specified. If a backup file with the same name already exists in the location selected, the system asks whether to overwrite the existing file.
- After backing up a directory, perform backups of project files and databases from individual software products that are participating in theFactoryTalksystem.If the applications include:
- HMI servers:Back upFactoryTalk Viewfiles separately. SeeFactoryTalk Viewdocumentation for help.
- Run theRSLinx Classicdata servers:RSLinxBackup Restore utility to back up the data server configuration. From themenu, selectWindowsStartRockwell Software >.RSLinx> Backup Restore Utility
- The base configuration of theFactoryTalk Linxservers:FactoryTalk Linxserver is included in the backup, including redundancy and alarms and events configurations.TIP:If theFactoryTalk Linxconfiguration option is not selected, make a copy of the fileRSLinxNG.xmland keep it with your backup archive to retain device, driver, and shortcut configurations. By default, the file is located inC:\ProgramData\Rockwell\RSLinxEnterprise.
- : OpenFactoryTalk LinxData BridgeFactoryTalk LinxData Bridge, selectFile > Export configuration. Keep the exported file with your backup archive.
- :FactoryTalk LinxGateway
- ForFactoryTalk LinxGateway version 6.20 and earlier, make a copy of theFTLinxGateway.xmlfile and keep it with your backup archive. By default, the file is located inC:\ProgramData\Rockwell\FactoryTalk Linx Gateway.
- ForFactoryTalk LinxGateway version 6.21, make a copy of theFTLinxGateway.dbfile and keep it with your backup archive. By default, the file is located inC:\ProgramData\Rockwell\FactoryTalk Linx Gateway.TIP:If there are two files named asFTLinxGateway.db-shmandFTLinxGateway.db-walunder the folderC:\ProgramData\Rockwell\FactoryTalk Linx Gateway, make a copy of these two files together withFTLinxGateway.dbfile.
- : The base configuration for the OPC UA Connector can be restored. After the restore operation is completed, you will need to regenerate a certificate and enter a password to return the OPC UA Connector to full operation.FactoryTalk LinxOPCUA Connectors
- Use MicrosoftFactoryTalk Alarms and EventsLogs:SQL Server®tools to back up and restore database files.
- : Back up project files using theFactoryTalk Transaction ManagerConfigurationmenu. SeeFactoryTalk Transaction Managerdocumentation for help.
- Copy theFactoryTalk Batch:FactoryTalk Batchfiles back to the same directory locations. SeeFactoryTalk Batchdocumentation for help.
- Other products: Back up product-specific information separately. See product documentation for help.IMPORTANT:FactoryTalk Services Platform6.10 applies a new encryption algorithm to the backup file for enhanced security. Backups created usingFactoryTalk Services Platform6.10 can only be restored to host computers that are also runningFactoryTalk Services Platform6.10 or later. Backups created usingFactoryTalk Services Platform2.90 or later can be restored onto host computers that are runningFactoryTalk Services Platform6.10.
Provide Feedback