RSSecurity Migration Utility
How do I open RSSecurity Migration Utility?
To open the RSSecurity Migration Utility:
- SelectStart > All Programs > Rockwell Software > FactoryTalk Tools > Import RSSecurity Configuration.
- Complete theImport an RSSecurity databasedialog box, then clickNext.
Use
RSSecurity Migration Utility
to choose whether to preserve existing RSSecurity groups and import them as FactoryTalk
groups, or import the items from RSSecurity groups as individual actions or resources. For more information about the imported groups, refer to Locations and permissions of imported resource and action groups.Import RSSecurity action groups and resource groups as
FactoryTalk
action groups and resource groupsChoose this option only if all computers in the
FactoryTalk
system have been upgraded to FactoryTalk Services Platform
2.10 or later. This option preserves RSSecurity groups and imports them as FactoryTalk
groups. The import process:- imports resource groups by associating individual resources with selected applications or areas
- places action groups, with associated individual actions, into theAction Groupsfolder in theFactoryTalk Directory
Import RSSecurity action groups and resource groups as individual actions or resources
This option breaks RSSecurity groups apart and imports actions and resources into the
FactoryTalk Directory
as individual, ungrouped items. The import process places these individual resources (with associated actions) under the Networks and Devices
folder in the FactoryTalk Directory
.Import example

Provide Feedback