Resolve issues with the import (Import Issue Resolution dialog box)
While importing an
RSSecurity Server
database, conflicts occur that must be resolved before the import can continue. If there are conflicts, the Import Issue Resolution
dialog box opens.To refer to import issues later, open the import log file. This file is located in the same location as the database .bak file.
To resolve issues with the import
- Do one of the following:
- To change an action, select the action, and then select a different action in the list. See descriptions ofMerge,Replace, andSkipbelow.
- To rename an item, in theNew namecolumn, enter a new name for the item. See the description of theRenameaction below.
- To close theImport Issue Resolutiondialog box, selectContinue.
To resolve issues with items that already exist
If a user group, for example one named Operators, already exists in
FactoryTalk Directory
, decide whether to:- Mergethe two user groups with the same name
- Renamethe RSSecurity user group
- ReplacetheFactoryTalk Securityuser group
- Skipimporting the RSSecurity group
Merge the two user groups with the same name
Merge the RSSecurity user group with an existing
FactoryTalk Security
user group of the same name. Example: Merge members of an RSSecurity Operators group with members of a FactoryTalk Security
Operators group:- User accounts in the RSSecurity groupthat do not existin theFactoryTalk Securitygroupare addedto theFactoryTalk Securitygroup.
- User accounts in the RSSecurity group thatalready existin theFactoryTalk Securitygroupremain unchangedinFactoryTalk Security. They are not overwritten.
- User accounts already present in theFactoryTalk Securityuser group but that do not exist in the RSSecurity groupremain unchangedin theFactoryTalk Securityuser group.

Rename the RSSecurity user group
Rename the RSSecurity user group to import the RSSecurity user group into
FactoryTalk Security
with a new name. Any security settings associated with the RSSecurity user group are transferred to the FactoryTalk Security
user group with the new name.
Replace the
FactoryTalk Security
user groupReplace the
FactoryTalk Security
user group with the RSSecurity user group. The original FactoryTalk Security
user group is deleted and replaced by the RSSecurity group. All security permissions associated with the original FactoryTalk Security
user group are also deleted.
Skip importing the RSSecurity user group
Skip importing the RSSecurity user group. This skips importing any other security settings that refer to the user group.
Example: If a resource defines security settings for the skipped user group, the resource will be skipped as well - there is a RSSecurity computer group named action. If importing the
Runtime Workstations
and an RSSecurity resource named MY_PLC5
that references the computer group. The MY_PLC5
resource is granting all users from Runtime Workstations
the RSLogix 5
\Go OnlineRuntime Workstations
group is skipped, the MY_PLC5
resource referencing the group is also skipped. This means that none of the permissions assigned to the MY_PLC5
resource are imported.
Provide Feedback