Import log file

The
FactoryTalk® Security
Import tool creates a detailed log file in plain text format, containing information about the import. Use a text editor to view the contents of the log file.
The log file is located in the same folder as the database backup (*.bak) file imported. The log file is overwritten every time the same database backup file is imported. The log file has the same name as the database backup file, but adds "(Import Status)", and has a *.txt extension. For example, if the database backup file is named MyDatabase.bak, the log file is named MyDatabase(Import Status).txt.
Information
Section
The RSSecurity Server database file (*.bak) imported.
PARAMETERS
What information the database file contained.
LOADING BAK FILE
What changes were made to the data before it was imported.
VALIDATING CONFIGURATION
Warnings or errors encountered during importing.
IMPORTING USERS
IMPORTING USER GROUPS
IMPORTING WORKSTATIONS
IMPORTING WORKSTATION GROUPS
IMPORTING ACTIONS
IMPORTING ACTION GROUPS
IMPORTING RESOURCES
IMPORTING RESOURCE
The result of the import, including whether it succeeded or failed, or whether it was cancelled.
DONE
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal