FactoryTalk Security benefits over RSSecurity
Consider migrating to
FactoryTalk® Security
, if currently using RSSecurity Server.FactoryTalk Security
offers the following benefits:- Centralized administration.Instead of maintaining lists of user, computer, and group accounts in each product, and then duplicating these lists in RSSecurity Server,FactoryTalk Securitydefines users, computers, and groups only once, and then maintains them in one place.
- A central authority for security.Instead of defining portions of your security system in individual products, and then portions of the system in RSSecurity,FactoryTalk Securitydefines security for allFactoryTalkproducts in one place. Users can log on and be authenticated by one central authority - theFactoryTalk Directory- regardless of which product used to access theFactoryTalksystem.
- Get your system running, or make changes, quickly without duplication of effort.RSSecurity Server requires setting up individual products, and then defining securable actions and resources for them, such as reading or writing values in data servers. WithFactoryTalk Security, a complete list of securable actions is available automatically for every product that supportsFactoryTalk Security.
Provide Feedback