Select an HMI device
The screens in a project represent the physical size of the HMI device selected for the project.
Use the
Application
tab of the Project Properties
dialog box to:- Specify the location of the HMI device to which the runtime application will be downloaded.
- Select the type of HMI device for the project.
- Specify how screens scale inView Designerif you change the target HMI device after you create screens for a project.
- Specify how screens scale if you download a runtime application to an HMI device that has a different size or aspect ratio than the HMI device for the configured project.
Provide Feedback