Application tab

How do I open the Application tab?
On the
Menu
bar, click
Project > Project Properties
and click the
Application
tab.
  • Use the
    Application
    tab of the
    Project Properties
    dialog box to:
    • Specify the location of the HMI device to which to download the runtime application.
    • Select the type of HMI device for the project.
    • Specify how existing screens scale in
      View Designer
      when changing the target HMI device.
    • Specify how screens scale when downloading a runtime application to an HMI device that has a different size or aspect ratio than the HMI device for the configured project.
    • Specify the size of the keyboard and keypad for the HMI device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal