Select a target HMI device for a new project
The screens in a project represent the physical size of the HMI device selected for the project.
Prerequisites
- Create a new project. SelectingFinishon theNew Projectdialog box opens theProject Propertiesdialog box.
To select a target HMI device for a new project:
- On theProject Propertiesdialog box, click theApplicationtab.
- In theLocationbox, select from a list of the most recently used location.TIP:When clickingBrowse
to select the HMI device, the OKbutton is available only when aView Designer-compatible device is selected. - In theTypebox, selectBrowse
. - On theSelect HMI Devicedialog box, select the appropriate HMI device type. By default, this is the HMI device type specified in theNew Projectdialog box.
- SelectOK.TIP:Use theScreen Scalingoptions on theApplicationtab when changing the HMI device type after creating screen content.
Provide Feedback