Change the target HMI device for a project and select a Screen Scaling option
The screens in a project represent the physical size of the HMI device selected for the project.
Screen Scaling
option.
IMPORTANT:
- Changing the screen size and then changing it back to the original size may change the size and position of the contents.
- Changing screen size cannot be undone. To revert to the original screen size, change to the original screen size.
To change the target HMI device for a project and select a Screen Scaling option
- Open the project.
- (optional) To save the project with a new name to preserve screen content in the original project, on theMenubar, selectFile > Save Project As, enter a new name, and selectSave.
- On theMenubar, selectProject > Project Propertiesand select theApplicationtab.
- In theTypebox, selectBrowse. TheSelect HMI Devicedialog box opens.
- Select the appropriate HMI device type. The default HMI device type is set in theNew Projectdialog box.
- SelectOKto close theSelect HMI Devicedialog box.
- In theScreen Scalingsection of theApplicationtab, select a scaling option:
- Screen content anchors to the upper left of the screen. Any extra space appears to the right of or below the converted screen content.
- Scale with fixed aspect ratio.(Default) When you resize the screen, content is resized to fill the screen as much as possible while maintaining the same aspect ratio. If the aspect ratio of the screens changes from regular (4:3) to wide, or vice versa, squares and circles do not elongate into rectangles and ellipses.
- In addition, wrapped text may wrap at different word boundaries on the new screens.
- Stretch to fit.Resizes the screen content to fill the screen. As you resize the screen from wider or narrower and vice versa, squares and circles are elongated into rectangles and ellipses.
- Screen content ianchores to the upper-left of the screen. Any extra space is added to the right of or below the converted screen content. If the screen on a new
- Do not scale.Keeps the screen content the same size and position on the new HMI device as the original screens.
PanelViewHMI device is smaller than the original screen, the content might be placed outside the new screen borders.
- In theKeypad and Keyboard Sizesection, select the size of the keypad and keyboard for anPanelView5000 device.
- Normal. The default size of the keypad and keyboard.
- Large. The keypad and keyboard display in a larger size similar to a physical keypad and keyboard.TIP:The HMI device scales theLargekeypad and keyboard to fit the screen.
- SelectApplyand then selectOK.TheProject Propertiesdialog box closes.TIP:Tips:
- Changing the target HMI device to an HMI device that allows fewer controller references displays errors on theReferencestab of theProject Propertiesdialog box.
- The maximum number of controller references for the HMI device appears at the top of theReferencestab.
- Delete controller references on theReferencestab to not exceed the maximum allowed for the HMI device of the project.
- Review the screens, popups, and the banner in the project to ensure that the content, including text and raster images, displays as intended.
Provide Feedback