Project Properties dialog box
How do I open the Project Properties dialog box?
On the
Menu
bar, click Project > Project Properties
. The
Project Properties
dialog box consists of:- Applicationtab: Select or change the target HMI device for a project.
- Referencestab: Add and configure the controller references for a project.
- Log On Methodtab: Select the logon method for users of the HMI device.
- Languagetab: Select the default language for HMI devices to use for a download or restart.
- Input Methodtab: Select the default input method for HMI devices.
- Usage & Capacitytab: Compare the total number of user-defined screens and popups as well as the total number of controller references in the open project with the maximum number allowed. View the number of existing shortcuts, Add-On Graphics, PDFs, and images used in a project.
Provide Feedback