Add a controller reference
A controller reference is a connection to a
Logix Designer
project file (.acd) from a View Designer
project file (.vpd). The connection automatically synchronizes data between a Logix Designer
project file (.acd) and View Designer
project file (.vpd). For PanelView
5510 HMI devices, View Designer
supports up to four controller references. Adding a controller reference adds the controller reference to the next available reference card on the .
References
tab. Each controller reference has a number in the reference card. This controller number appears when browsing for HMI device controller tags in the Tag Browser
IMPORTANT:
Select a controller only from an Ethernet network. Logix controllers and project files must be version 27 or later.
TIP:
For projects with a
PanelView
5000 HMI device, the recommended number of tags across all four Logix controllers is 200,000. A tag is a scalar tag. Scalar tags are BOOL, DINT, REAL, a member of structure, or an element of an array.To add a controller reference
- On theProject Propertiesdialog box, select theReferencestab.
- In theController[#] Reference Namebox, type a unique name for the controller reference. Name the controller reference a different name than the project.TIP:Tips:
- Add up to four controller references for projects configured with aPanelView5510 HMI device.
- Entering a controller reference name or selectingAdd controller reference
adds an additional controller reference card for projects configured with a PanelView5510 HMI device. - Added controller references appear after the last controller reference card. After saving controller references, reference cards appear in order by controller reference number that appears in theController[#] Reference Namebox.
- Adding the maximum number of controller references for an HMI device makesAdd controller reference
unavailable. - Add up to four controller references for projects configured with aPanelView5510 HMI device.
- Entering a controller reference name or selectingAdd controller reference
adds an additional controller reference card for projects configured with a PanelView5510 HMI device. - Added controller references appear after the last controller reference card. After saving controller references, reference cards appear in order by controller reference number that appears in theController[#] Reference Namebox.
- Adding the maximum number of controller references for an HMI device makesAdd controller reference
unavailable. - Controller References each contain an index number. When controllers replicate at the same time, the controller with the lowest index number replicates before the other controllers in queue. The controller with the lowest index number in queue has the highest priority.
- The combined number ofPanelView5000 HMI devices and Logix controllers that can communicate with each other through a 1756-EN2T or 1756-EN3T Ethernet module is eight or fewer.
- Type the path of the file or select a Logix Designer project file (.acd) by selectingBrowse
next to the Logix Project Filebox.TIP:The project file (.acd) for each referenced controller must beLogix Designerversion 27 or later. - Set the path from the HMI device to the controller:
- Type the IP address of the controller. To browse for the controller, after theHMI to Controller Pathbox, selectBrowse
and select the controller running the selected Logix Designer project file (.acd). - In theSlotbox, select the slot number of the controller to reference. After browsing to the controller in the previous step, the slot number appears automatically.
- Set the path from theView 5000 Emulatorto the controller:
- After theEmulator to Controller Pathbox, selectBrowse
and select the controller running the selected Logix Designer project file (.acd). - (optional) If the controller is previously viewed, select theSelect Controller Pathlist and select the controller from an Ethernet network or virtual backplane running Logix Emulator.TIP:Tips:
- TheSelect Controller Pathlist contains up to the last five recently viewed controller paths. If there are no previously viewed paths, the list does not appear.
- Setting the Emulator to Controller path to the same path for multiple controller references displays duplicate alarms in the Alarm Summary and the Alarm Manager. Each alarm in the controller displays for each controller reference that has the same Emulator to Controller path.
- SelectApplyto save changes and keep theProject Propertiesdialog box open, or selectOKto save changes and close the dialog box.TIP:When browsing for a controller, theOKbutton is available when selecting aView Designer-compatible device.
Provide Feedback