Work with controller references
A controller reference is a connection to a
Logix Designer
project file (.acd) from a View Designer
project file (.vpd). The connection automatically synchronizes data between a Logix Designer
project file (.acd) and View Designer
project file (.vpd).Add up to four controller references, and a recommended maximum of 50,000 tags in a Logix controller to a project. Use a maximum of one controller for each
PanelView
5310 project or a maximum of four controllers for a PanelView
5510 project.
TIP:
Every scalar, array element, and structure member is considered a separate tag.
Use the
References
tab on the Project Properties
dialog box to add or change a controller reference.Provide Feedback