References tab
How do I open the References tab?
- ClickVIEW > Project Explorer.
- Right-click the project name.
- SelectProject Properties.
- Click theReferencestab.
Use the
References
tab to add controller references to the project. A controller reference is a connection to a Logix Designer
project file (.acd) from a View Designer
project file (.vpd). Add up to four controller references for a PanelView
5510 HMI device. The connection automatically synchronizes data between a Logix Designer
project file (.acd) and View Designer
project file (.vpd).Provide Feedback