Copy a controller reference
Copy a controller reference within a
View Designer
project or from one View Designer
project to another. This eliminates the need to manually enter the information in a project. Copy individual items from a controller reference or the entire controller reference. Paste controller references that are of the same version of Logix Designer
.Prerequisites
- Open the sourceView Designerproject containing the content to copy.
- If pasting content into another project, start an instance ofView Designerand open the target project. Open no more than three instances ofView Designerat one time.
To copy a controller reference
- In the source project, selectProject > Project Propertiesand select theReferencestab.
- Right-click the controller reference and selectCopy.TIP:To copy a single item from a controller reference card, select the controller reference, select the item to copy, and then right-click and selectCopy.
- In each target project:
- SelectProject > Project Propertiesand select theReferencestab.
- Right-click the new controller reference card and selectPaste. Pasting assigns the next available controller reference number.
- SelectApplyto save changes and remain on theProject Propertiesdialog box, or selectOKto save changes and close theProject Propertiesdialog box.TIP:Tips:
- Pasted controller references appear after the last controller reference card. Each controller reference card has a controller reference number that identifies the position on theReferencestab and the name of the referenced controller. When reopening theReferencestab, reference cards appear in order by controller reference number that appears in theController[#] Reference Namebox.
- After saving controller references, reference cards appear in order by controller reference number.
- ForPanelView5310 HMI devices,View Designerdoes not support pasting a controller reference in a project that already contains a controller reference.
- ForPanelView5510 HMI devices, paste up to four controller references in a project.
- For multiple controllers and their tags to appear in thefor aTag BrowserPanelView5510 HMI device, the project file (.acd) for each referenced controller requires the same version ofLogix Designer.
- View Designerdoes not support pasting a number of controller references that exceeds the total allowed for an HMI device. A prompt appears to paste the copied controller references that do not exceed the maximum for the HMI device.
- The maximum number of controller references appears at the top of theReferencestab and on theUsage & Capacitytab. Deleting the required number of controller references from theReferencestab removes the errors.
Provide Feedback