Browse for Controller window
In the
References
tab of the Project Properties
dialog box, or on the Controller References
page of the Download
wizard, click Browse
next to the Slot
box. The
Browse for Controller
window is a network browser that displays active network connections and devices in tree form. Use the
Browse for Controller
window to select a controller to reference for the project.Provide Feedback