Remove an HMI device from the network tree
Remove an HMI device from the network tree in the
Browse HMI Device
window to display only the devices relevant to the project. To remove an HMI device from the network tree
- On theApplicationtab of theProject Propertiesdialog box, or on theHMI Device Locationpage of theDownloadwizard, selectBrowsenext to theLocationbox.
- In theBrowse HMI Devicewindow, right-click the HMI device and selectRemove.
Provide Feedback