Browse for HMI Device window

In the
Application
tab of the
Project Properties
dialog box, or on the
HMI Device Location
page of the
Download
wizard, click
Browse
next to the
Location
box.
The
Browse for HMI Device
window is a network browser that displays active network connections and devices in tree form.
Use the
Browse for HMI Device
window to:
  • Select a target HMI device to which to download the project.
  • Remove an unused HMI device from the network tree.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal