Usage & Capacity tab

How do I open the Usage & Capacity tab?
On the
Menu
bar, click
Project > Project Properties
and click the
Usage & Capacity
tab.
The
Usage & Capacity
tab compares the number of certain items included in the open project with the maximum number allowed in a project. Use this tab on the
Project Properties
dialog box to:
  • Compare the total number of user-defined screens and popups in an open project with the maximum number allowed for a project.
  • View the number of existing shortcuts, Add-On Graphics, PDFs, and images used in an open project.
  • Compare the size of the data log configuration in an open project to the maximum size allowed for a project.
  • Compare the total number of controller references in an open project with the maximum number allowed for the selected HMI device of the project.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal