FactoryTalk ViewPoint Help
FactoryTalk®
ViewPoint is an add-on to FactoryTalk View
that serves fully animated, read and write displays of FactoryTalk View
applications to a web browser. Published displays are accessible on demand, with no additional Rockwell Automation
software required.FactoryTalk ViewPoint
applications are served from a dedicated host computer. When connected to the FactoryTalk ViewPoint
server's network, simply open a browser on your desktop or mobile device, enter the computer name or IP address of the FactoryTalk ViewPoint
server, and view live information about your plant or process.Rockwell Automation
recognizes that some of the terms that are currently used in our industry and in this publication are not in alignment with the movement toward inclusive language in technology. We are proactively collaborating with industry peers to find alternatives to such terms and making changes to our products and content. Please excuse the use of such terms in our content while we implement these changes.Provide Feedback