FactoryTalk ViewPoint mobile interface
The mobile interface is designed for viewing displays, alarms, and recipes on mobile phones and tablets. The mobile interface automatically scales itself and the active display to the size of your device.
The
FactoryTalk ViewPoint
mobile interface is supported for published FactoryTalk View SE
applications only.Provide Feedback