Recipes page
How do I open the Recipes page?
- From the mobile menu or title bar, selectRecipes, select an HMI server, and press
.
The
Recipes
page in a web application shows the defined recipes on the HMI server. Use the Recipes
page to view, download, and quickly filter recipes.The
Recipes
page shows only when you are granted the RecipePro: Preview
permission in FactoryTalk Security
.

Item | Description |
|---|---|
![]() | This is the Quick Filter box. In this box, type the text to show the recipe files or recipes that match the text. Recipe files or recipes are filtered as you type. |
![]() | This area shows all the recipe files on the selected HMI server. |
![]() | This is the Select HMI Server icon. Press this icon to select an HMI
server. |
![]() | This area shows all the ingredients in the selected recipe file. |
![]() | This is the Download recipe icon. Press this icon to write the ingredient
values of the selected recipe file to the tags in the tag set. |
![]() | This is the More information icon. Press this icon to show more information about the selected recipe file. |
![]() | This is the Refresh icon. Press this icon to show the latest recipe
information and current values on the page. |
Provide Feedback