Alarm priority and state icons
The following table describes the alarm priority and state icons.
Icons | Priorities and states |
|---|---|
![]() | Urgent priority |
![]() | High priority |
![]() | Medium priority |
![]() | Low priority |
![]() | Event priority |
![]() | Active 1 |
![]() | Active and suppressed 1 |
![]() | Inactive 1 |
![]() | Inactive and suppressed 1 |
![]() | Inactive and disabled 1 Inactive, disabled, and suppressed 1 |
![]() | In alarm and unacknowledged |
![]() | In alarm, unacknowledged, and shelved |
![]() | In alarm, unacknowledged, and suppressed In alarm, unacknowledged, suppressed, and shelved |
![]() | In alarm and acknowledged |
![]() | In alarm, acknowledged, and shelved |
![]() | In alarm, acknowledged, and suppressed In alarm, acknowledged, suppressed, and shelved |
![]() | Normal and unacknowledged |
![]() | Normal, unacknowledged, and shelved |
![]() | Normal, unacknowledged, and suppressed Normal, unacknowledged, suppressed, and shelved |
![]() | Normal and acknowledged |
![]() | Normal, acknowledged, and shelved |
![]() | Normal, acknowledged, and suppressed Normal, acknowledged, suppressed, and shelved |
![]() | Normal, unacknowledged, and disabled Normal, unacknowledged, disabled, and suppressed Normal, unacknowledged, disabled, and shelved Normal, unacknowledged, disabled, suppressed, and shelved Normal, acknowledged, and disabled Normal, acknowledged, disabled, and suppressed Normal, acknowledged, disabled, and shelved Normal, acknowledged, disabled, suppressed, and shelved |
![]() | Bad quality |
| |
Provide Feedback
























.